Other Parts Discussed in Thread: TPS54319, TPS54540
TPS54319的DC/DC电路用于提供3.3V给系统的3G模块。TPS54319的输入电压5V,工作频率设为600KHz。
3G模块待机时,只消耗150mA电流,此时电路板发出细细尖尖的“啸叫”。
如果系统没有插3G模块,就不会听到“啸叫”。
请问为什么会发生“啸叫”?
具体电路参考附件。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 将输出22uf电容换成220uF/25V电解电容,结果还是有“啸叫”。
2. 电感也有换成4R7及2R2的,还是会“啸叫”。
3. 输入端增加电解电容,也是一样。
4. 24页的公式看了,但是设计的细节真的不知道怎么估算,有待请教。
我选的频率是600KHz,输入电压5V,输出3.3V。
5. 输出端依次接5欧姆,或是2.5欧姆水泥负载电阻,都不会有啸叫。
6. 输出端接华为MU609 3G模组,或是同时并联一个2.5欧姆水泥电阻,都会有啸叫。
测试了输出端的纹波图,有一个8KHz左右的周期噪音信号。
具体参考附件。附件中图片的横向时间轴,每格是50us;纵向是纹波电压,没格50mV。
电感换成屏蔽电感,绕线电感要浸漆。由于3G模块的电流是脉动的,会导致绕线电感或者瓷片电容发出响声。
观察下Vout的AC纹波大小,该低频纹波,一般有两个原因:电压本身不稳定或者输出动态响应慢,都需要调补偿环。建议结合Webench来调整补偿环路。
由于3G模块有循环突发动作,瞬间电流比较大, 要求3.5A以上的DC/DC 电源。
后来换成tps54540模块供电, 啸叫的声音有所减小,但还是有。