Other Parts Discussed in Thread: TPS40200
图片出自TPS40200的DATASHEET 。
图中注视了,我更换的器件,只有两处不同。
现在问题是:当我的输入电压慢慢的提高到28V左右,输出电压就降为0V, PIN6 DRV输出振荡的波形最低电平大于或者接近20V(示波器测量) 。会不会因为SI9407的G端电平是+ -20V。为何典型应用图中是这么使用?
为何不能实现典型应用图中的18~52V的输入范围?要怎么样改才能完成功能
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
能否告知该线路是否基于评估板修改的么? 若是自设计的, 能否提供pcb布线?
VDRV电压为VDD 与VDD-10 的PWM波形, 因此, PIN6 DRV输出振荡的波形最低电平大于或者接近20V(示波器测量)为正常现象.
这里输出电压改为5V, 电流纹波会相应增大,特别是输入电压增加情况下.若电流采样处理不好, 会使采样电流上噪声过大,从而误进入过流保护模式. 可以看一下PIN2和Vout 电压是否和Figure 26类似. 图中C8, C5应尽量靠近芯片引脚.
根据工程师的建议,电路问题主要是由于您的 PCB layout。下面是工程师给您的几点建议,供您参考,希望可以帮到您。
1. The feedback trace goes just underneath the switch node. Suggest customer flying the feedback wire (connect to output capacitor directly). The sensed voltage should be from the output capacitor, not the output of the inductor, it will also introduce noise and have bad regulation. Also, try adding a 100nF capacitor from the joint of R7 and R8 to the GND of IC.
2. GND connect is not good. The power GND and signal GND doesn’t seperated. Thus, the circuity is more sensitive to the noise. Also, single point should be considered in the design.
请您参考TI Datasheet中的PCB layout, 尤其是 the Kelvin Ground 和 the Kelvin sense. 特别注意在“Layout Hints”中的描述。
您的问题比较具体,如果上述建议还是不能解决问题,我们建议您能与当地代理商的现场工程师联络一下,现场看看具体情况。