Other Parts Discussed in Thread: DCR010505, TPS55010, LM2841
现在用的是ME7660 问题是5v输入 带载能力差,输出达不到-5V 顶多-4.25V 负载电流大概在3mA以内.
请大家帮忙!谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
你可以使用隔离模块DCP010505/DCR010505,将输出端Vout链接次级地,输出0V端相对于地为-5V。
你也可以使用其它隔离结构如fly-buck(TPS55010) flyback.
或者你可以考虑用buck芯片做buck-boost.