This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2661-3-4EVAL: +12V转-12V器件选型--LM2661

Part Number: LM2661-3-4EVAL
Other Parts Discussed in Thread: THS3491, LM27761, LP2992, LM1117, LM2611

急急急!老师们好,现在我需要使用THS3491这款芯片,打算用±12V供电,目前我只有+12V的电源,想使用逆转芯片将其转换成-12V,经过调研打算使用LM2661
我目前的一套电源转换流程是这样的:

LT1962:12V-->5V
LM27761:5V-->-5V
LT1964:-5V-->-2.5V
LP2992:12V-->5V
LM1117:5V-->2.5V
 
我看到LM2661应该是可以实现我需要的功能,我看到一个典型的应用是12V转-5V,也说了通过配置RFB2可以调整输出电压,我的理解是这样子的:VOUT = -1.22(参考电压) * (RFB2/RFB1)* VIN ,那也就是说如果我需要-12V输出,我应该将RFB2配置为24K,不知道我理解的是否正确