This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PFC用ucc3818芯片,一上电后驱动就有一个8ms的打开时间,导致MOS管炸,为什么呢?

Other Parts Discussed in Thread: UCC3818

近做一个2500W的PFC电路,用的ucc3818芯片,一上电后驱动就有一个8ms的打开时间,导致MOS管炸,为什么呢?

图中,黄色代表芯片的驱动波形,蓝色是输出400V波形。

具体情况为:输入120V,防浪涌电阻给大电容充电,然后继电器吸合,刚一吸合后,就会有一个8ms的驱动时间,因为我加的电压低,MOS管还撑得过去,之后有一个大约0.9s的软启动,之后电压就慢慢升到400V。

想问一下,为什么会有一个8ms的驱动波形?