This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756EVM: Does BQ25756 Support Current Calibration? EVK Shows Over 100 mA Offset

Part Number: BQ25756EVM
Other Parts Discussed in Thread: BQ25756

Hello,

I would like to confirm whether the BQ25756 supports any form of current calibration (for charge current, input current, or system current).

I am currently using the BQ25756 EVM, but I am observing a consistent offset of more than 100 mA between the measured current and the actual current. This level of deviation will affect the accuracy of my application’s power and energy calculations.

Is there any calibration method, register adjustment, or recommended procedure to reduce this measurement offset? Or is this level of tolerance expected for the device?

Thank you.