tps61165芯片的典型应用是背光升压电路,我把它当做了一个输出固定电压的升压电路。输入3.3V输出10.4V,常温下挂着负载10.4V可以输出正常,但是低温情况下,刚上电加着负载就输出不正常了,输出只能达到4V左右的样子。把负载去掉后,10.4V输出又正常了,在不断电的情况下,再挂上负载,10.4V输出正常。感觉是启动的时候,负载电流太大造成的,但是这个负载的工作电流只有50mA。不知道这是为何?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
将输入电容加大一点,例如10uF.
layout上尽量靠近芯片Vin脚和电感输入端?
输入电压拉低,更容易过流保护,甚至欠压保护。
Hi
低温下,要注意电容溶值是有下降的,可能存在电压不稳的情况。
可以测量一下PWM波形,低温下,有可能是不稳定导致启动不了,比如电容在低温下容值会急剧降低。