Other Parts Discussed in Thread: TPS61093-Q1
TPS61093-Q1的PIN7(FB)端电压偏离资料给出的0.5V,PIN7相连的电阻串为2.2KΩ/51KΩ时,PIN7电压1V,输出19V;电阻串10KΩ/100KΩ时,PIN7电压1.9V,输出电压约18.6V,是否芯片已坏。
输出电流与PIN7电阻网络电流有何关系。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS61093-Q1
TPS61093-Q1的PIN7(FB)端电压偏离资料给出的0.5V,PIN7相连的电阻串为2.2KΩ/51KΩ时,PIN7电压1V,输出19V;电阻串10KΩ/100KΩ时,PIN7电压1.9V,输出电压约18.6V,是否芯片已坏。
输出电流与PIN7电阻网络电流有何关系。
Hi
FB电压并非芯片输出,而是输出电压分出来的,与芯片内部的参考电压0.5V做误差放大。
测试一下FB阻抗是否异常,有可能烧掉了。(注意FB的低边电阻选择,一般是10kohm,可以小一点,不能像其他芯片那样选择很大的电阻))
Hi
FB电压并非芯片输出,而是输出电压分出来的,与芯片内部的参考电压0.5V做误差放大。
测试一下FB阻抗是否异常,有可能烧掉了。(注意FB的低边电阻选择,一般是10kohm,可以小一点,不能像其他芯片那样选择很大的电阻))
多谢。
设计目标是5V输入,12V/50mA输出。目前选用了人,2.2Kohm/51Kohm的电阻分压。
请教一下:输出电流如何计算,datasheet中不是很清楚,FB端限流是100uA,与输出电流有关联吗?