用tps563200输入9v,输出4.1v,原理图如下:
tps563200带载波形为:
用LM2596带载波形做对比:
不想用LM2596的原因是因为其功耗大,封装大。
真心想调好TPS563200,按说带载能力两个都是3A,但是波动实在相差很大。
希望给予指导与建议,谢谢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主试试把时间轴调小,抓一下电压在加载瞬间的突变波形看看
yang zhang18 说:从tps563200带载波形看,4.27v供电给负载,负载启动时会有600mv的降低,持续将近25s;负载运行后也有将近240mv的降低到4.03v左右供电。
而LM2596带载波形看,负载启动时只有120mv的降低,持续将近25s;负载运行后也有将近40v的降低到4.23V左右供电。