Other Parts Discussed in Thread: BQ24295, BQ24296, BQ2000, BQ24650, BQ24172, BQ24170
| 找一个单节的充电IC; 开关型(输入电压提供5V@1A时,输出1A时输入电流应小于输出电流); 支持CC-CV模式,另外CV电压能够设置,最好范围支持到钛酸锂2.7V到钴酸锂4.3V; 能够独立工作; 有没有合适的型号给推荐? |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeleon
想问一下楼主
钛酸锂电池的截止电压是2.7V吗?
目前推荐您使用的IC是BQ24295,截止电压可以从3.5V调制4.4V
http://www.ti.com/lit/ds/symlink/bq24296.pdf
通过Ilim Pin 直接通过电阻设置限流即可,
如果需要调整截止电压参数则需要I2C来修改参数。
谢谢!
Hi
BQ24296是可以通过不接I2C来使用的,只是默认的截止充电电压为4.2V
如果完全要不适用MCU,可以用BQ24172,带FB反馈引脚
http://www.ti.com/lit/ds/symlink/bq24170.pdf
谢谢!