Other Parts Discussed in Thread: BQ24072, BQ24072T
电路图是根据datasheet上面给的典型应用画的,在Vbat插入电池后,两个状态指示灯都是可以亮的,但是电源上就是没有充电电流,电池已放电到3.3v以下了。
EN1,2、TD、CE都是同时接的低电平。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
5V插进来的时候,OUT有输出电压吗?接上电池以后,没有充电电流,这个时候OUT电压又是多少?
另外,你量一下TS脚的电压是多少?
我是在输出后面截了一个开关电源,所以不管是否接了电池,输出都保持在3V。
而TS脚的电压是0V左右,这个有问题吗?
如果输出有,说明芯片工作正常。不能充电和TS电压有关系。TS用来判断电池温度是不是过高或过低,如果TS电压是0V,芯片会认为电池太热,当然不给电池充电了。TS脚你还是要接个电阻。
TS脚我是接了一个10K的电阻到地了,还是不行啊。我今天发现当TS脚是0.6-1.1V的时候,电源就会有电流输出。但是我觉得这个范围太小了把,datasheet上给的是0.3-2V把
你如果接了10k电阻到地了,为啥TS脚测出来的电压会是接近0V呢?我算下来怎么也是在750mV左右的。
现在的问题点,就是出在TS脚的电压上,电压对了,就能充电了。
你是怎么测的TS脚电压范围对充电的影响?如果拿电源直接加,这个是不推荐的。还是拿电阻接上验证好一些。不用纠结你测的值为啥和规格书上的不一样。
是的,问题就是在TS的电压上。我确定我是在TS脚接了10K电阻到地,但是TS脚就是没有电压,这点我也是很疑惑。所以就用电源直接加上去,发现就有充电电流了。我想是不是有可能我在吹芯片的时候,把片子吹坏了?温度是390
一般用风筒不至于吹坏芯片。建议你:1)把芯片吹下来,重新再焊一边,看看有没有可能是虚焊或者是什么地方有连锡或者锡渣引起的;2)这样还不行,就换颗芯片试试,如果还是一样的问题,那我觉得是板子上的可能性大一些。如果换了就没问题了,那估计芯片被损坏的可能性大一些。
我想 应该不是虚焊的问题,因为好几块板子都出现了这个问题,但是我觉得就是TS上面的那个电流源没有工作了。我现在采取的方法是利用输入电压的电阻分压给TS脚加一个1V的电压。不过感觉这只是治标不治本,还是想知道最根本的问题出在哪。
你查一下料号,用的是BQ24072还是BQ24072T,这两个是不一样的。如果是BQ24072就不会出现你说的问题,如果是BQ24072T,那就是你说的这样,要外加分压到TS脚。我估计你用的应该是T版本。
好的谢谢了,还有一个问题,BQ24072T是不是就是没有带温控功能的了啊?
有温控的。温控包含两个方面,规格书上都有说明,一个是芯片的节温控制,如规格书第18页;二是电池温度检测,如规格书第19页。