This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090A: 关于UCD9090A的使用

Part Number: UCD9090A

您好!

有八路电源需要按序使能、逆序关闭。具体实现设想如下:

1、使用PMBus_CNTRL 作为总使能开始

2、当PMBus_CNTRL拉高后,第一轨EN对应的GPIO拉高,该轨电源器件开始上电,完成后电源输出PG有效(拉高)数字信号。

3、该PG数字信号接到UCD9090A的一路GPIO,UCD9090A由此确认该路电压上电完毕,开始第二轨使能

4、第二轨EN对应GPIO拉高,该轨电源器件开始上电,上电完成输出PG有效数字信号(拉高),并接到UCD9090A的GPIO,由此确认第二轨上电完毕,开始第三轨使能,以此类推到第八轨,前面七个轨道都是用被控电源的PG反馈到UCD9090A的GPIO判定上电完毕的。

5、第八轨对应EN拉高后,要同时使能另外9个电源器件,这9个电源没有PG输出功能,要把输出电压分别接到9个MON模拟输入,当9个电压都符合UV、OV设置后,UCD9090A用一路GPIO输出总PG信号。系统上电阶段完成,正常工作状态。

6、在正常工作状态,任意前面七路PG信号被拉低,或者第八路EN驱动的9个电源MON电压超差,UCD9090A的总PG信号无效,并拉低所有EN掉电。

7、当PMBus_CNTRL拉低后,UCD9090A开始下电,从第八轨开始依次逆序关闭EN.

请问以上设想是否可行?

谢谢!