Part Number: LM5022
Other Parts Discussed in Thread: PMP20128
各位工程师好,我用LM5022搭sepic电路是给BLDC电机母线供电,峰值功率18W左右,通过MCU输出可调占空比的PWM经过RC低通滤波和电压跟随器到LM5022的VFB引脚调节sepic输出电压,那我LM5022外围的PCB该如何布局布线?看到"AN-1557 LM5022 Evaluation Board"www.ti.com/.../snva203c.pdf中两层评估板是把欠压保护UVLO的下拉电阻RUV1、软启动Css电容、频率电阻RT的信号GND端单独铺一小块铜皮,然后单独单点接地到输入输出功率地GND的大铜皮上。
既然LM5022是PWM控制器,那输入输出电容GND和外置MOSFET电流采样RSNS的GND端就是功率GND;
其余的UVLO下拉电阻RUV1、软启动Css电容、频率电阻RT、反馈下拉电阻RFB1、VCC电容CF的GND端和LM5022第6pin GND,这些信号GND是不是应该单独铺一块铜皮,然后再单点连接到输入输出及电流采样功率GND的大铜皮上呢?且我PWM的RC滤波GND端和电压跟随器的GND又该如何接?那针对我的应用PCB层数该设多少?(我目前预计用4层PCB),如何更好地PCB Layout才能高度稳定可靠?要注意哪些细节?请指导,谢谢!