BQ25505上电一段时间内,VIN是正常的输入电压3.3V,VBAT_SEC上的电容正常充电。可是电容充到2V多的时候,输入突然降到0V,并且电容不再充电,这是怎么回事?测试输入的前级还是正常的。
VBAT_OK = 2.4V
VBAT_OK_HYST = 2.66V
VBAT_OV = 4.8V
MPPT = 68%
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ25505上电一段时间内,VIN是正常的输入电压3.3V,VBAT_SEC上的电容正常充电。可是电容充到2V多的时候,输入突然降到0V,并且电容不再充电,这是怎么回事?测试输入的前级还是正常的。
VBAT_OK = 2.4V
VBAT_OK_HYST = 2.66V
VBAT_OV = 4.8V
MPPT = 68%
你说的输入降到0是指输入电压?输入电压都没有了,不充电是肯定的。
输入变成0后,能自己恢复吗?还是说必须重启才能恢复?
如果输入前级是正常的,芯片输入电压不可能没有啊
我是将交流电压整流后送到BQ25505的输入端,交流电压还是正常的,但整流电压为0.
输入变成0后,不能自己恢复,这种现象每次启动一段时间后就会出现。
给个电路图吧,你们交流是怎么整流的?用二极管桥式整流还是别的方式?我的理解,只有BQ25505电流太大了才可能把输入拉死。如果没有大电流,那么只能是前级自己把电压关了。
把charger输入换成一个直流源还会不会充电过程中中断?
还有,你把充电后级的负载断开,就是两个负载开关的路径断开。你现在的问题是把输入给拉没了,charger一般没这么霸道。你只留下电池充试试看,如果能充那说明负载影响了输入,如果还断,换颗芯片试试。