如图所示,锂电池串联成组,每组约十几块单体,单体电压3.7V,每串联单体之间串联一开关,开关打算使用“TPS22959 5.5V ,15A ,4.4mΩ 导通电阻负载开关”通过back to back方式组成的双向开关,但是看其说明发现Vin和Vout电压范围为0.8-5.5V,而串联的电池形成电压为几十V,电池组负极和TPS22959 均接地情况下TPS22959 能应用于此场景么?还是说电压范围为0.8-5.5V指的是Vin和Vout之间压降?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如图所示,锂电池串联成组,每组约十几块单体,单体电压3.7V,每串联单体之间串联一开关,开关打算使用“TPS22959 5.5V ,15A ,4.4mΩ 导通电阻负载开关”通过back to back方式组成的双向开关,但是看其说明发现Vin和Vout电压范围为0.8-5.5V,而串联的电池形成电压为几十V,电池组负极和TPS22959 均接地情况下TPS22959 能应用于此场景么?还是说电压范围为0.8-5.5V指的是Vin和Vout之间压降?
谢谢!
TPS22959的耐压是6V, 指的是VIN到GND之间的电压差,如果TPS22959的GND都连接最低端的电池负极,会造成耐压不够损坏IC。
如果back to back的TPS22959单独并联在每一节,且GND连接一起并联的电池负极是可以的。 但驱动的参考电压需要保持一样。