您好,我用一个CPLD直接驱动Uc2709,UC2709炸了,CPLD损坏。然后给中间接了一个51K的电阻,2709损坏,CPLD完好。
请问,这个东西究竟应该如何使用。十分感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UC1707的模拟关断确实可以用于做过流保护(按照上述的电路), UC2709并没有这一块的电路,在您的应用中,即便出现大的电流,如果MOS没有被击穿导致电流从驱动G极灌入芯片UC2709 OUT是不足以让UC2709炸掉的。
UC2709被炸掉的原因除了来自MOS击穿导致的G极大电压大电流的原因之外,就是UC2709本身输出的大电流,如果MOS没有击穿的话。这个即是重点考虑的原因。
如果MOS有击穿的话,可以在您的电路中,输入仍加入高的51k电阻保护驱动输入芯片,断开MOS,输出,在UC2709的OUT输出接1k的电阻,1nF电容并联(模拟MOS), 然后控制UC2709输入信号(占空比输入,可以外加,也可以由CPLD输出), 观察UC2709 OUT输出是否有问题,如果UC2709仍然炸掉,说明UC2709质量有问题,如果输出正常(占空比),代表UC2709 OUT输出的电流太大导致的,这个时候您需要在OUT输出增加限流电阻,参照datasheet选择10欧姆,并并联二极管加快放电。
如果不是因为输出电流或者MOS击穿导致的,输入电压低于5.6V, 在增加51k限流电阻的基础上还是会炸芯片,代表很可能是芯片质量问题,目前市场上是很多伪劣芯片。建议您到TI授权代理商处购买,其中只有e络盟可以小批量购买, UC2709属于工业级别的芯片,购买2~3片验证。
TI授权代理商联系方法:
www.ti.com.cn/.../gencontent.tsp
点击“+”看到电话联系。