Other Parts Discussed in Thread: TPS54228, PMP15012, LMR14206, LM2585
各位大神好,本人初次接触电源管理芯片,现在想选一款+12V输入,-12V和+5V输出,功率可能10W左右。
我看了咱们TI的产品,感觉输出不是正就是负,没有同时输出正负的。
还有,能不能介绍一下非隔离式DCDC、电源管理解决方案、LDO、隔离式DCDC这都是应用在什么场合?百度过了,理解不深,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
建议使用两个芯片实现你的方案,12V转-12V 多大电流,12V转5V多大电流?
-12V电流不大,也就100mA吧,5V电流较大,按照2A吧,因为这个5V还要转变为3.3V为单片机供电
建议使用LMR14206来做-12V, 设计可以参考PMP15012。 12V转5V可以使用TPS54228。
Hi
或者用回扫式稳压器LM2585:http://www.ti.com.cn/cn/lit/ds/symlink/lm2585.pdf
电路参考第15页, 适当做些调整就可以的(改12V的绕组使得输出3.3V等)。