This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8711 mos管选型问题

Other Parts Discussed in Thread: DRV8711

本人需在1.5cm*1.5cm以内,且mos管两刀价格以内解决两个全桥驱动,

MOS管需要满足35V以上  每个6A以上  每个50nC以内,内阻需满足耗散要求(自然对流,温升40内为佳)

最好MOS不宽于DRV8711芯片宽度,四或六层板,底层不得放置IC

原本计划采用FDMQ86530,但采购困难且价格过高;可有高人指点?

  • Hi Di yang

    你可以看一看DRV8432是否适合你的应用。电压52V,RMS电流达到7A,峰值电流12A。双H桥。如果不合适,我们再看看帮你选择合适的MosFETs. 

  • 设计上需要采用DRV8711,64细分以上,设计必须要满足5A堵转的;但可以考虑DRV8432作为后级替代MOS管,但性能不是很理想~

    5A输出时,110m欧姆内阻是否大了些? 110*4*5^2=11W  温升11*13.3℃/W=146.3℃;应该不行的~;用mos管可以轻松控制在15mΩ左右,算上开关损耗也能压在5W以内。

    由于有8路电机,即使使用DRV8432,个人更倾向DSP软件细分,仪表放大回测电流,并除去DRV8711;但本人无权利改变控制板电路SPI接口(已经做好)