Other Parts Discussed in Thread: TPS54620, TPS54386, LM25116, LM5116, UCC27222, UC3842, LM5119, LM3000
要做一个两相的交错并联Buck变换器,求推荐一款控制芯片,谢谢。
另,要求的工作频率为500kHz,最大占空比为87%,我看满足这两个要求的控制芯片比较少,求有经验的高手推荐一款合适的芯片,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
看看TPS54620并联使用的设计文档: http://www.ti.com/lit/an/slva389/slva389.pdf 是否满足?
内置MOS的:TPS54386,600KHz;我认为500K是可以有一定范围的
外置MOS的LM5116和LM25116:一片工作在500K,另外一片SYNC管脚180度移相(反相器或RC移相或运放&比较器移相)做从机;BUCK拓扑上并联即可
外MOS加外驱动的:UCC27222预测栅驱动两路+控制器(UC3525/3842/3846等等)
做两级的:前面BUCK;后面加万能恒流、恒压控制器,LTC4000*2;成本略高
常规的以上四种
当然还可以非常规的:
1: 选一个 D 类音频功率放大器(TPA XXXX)+MCU
2: 选一个 电机驱动器(DRV XXXX)+MCU
3:选一个 序列发生器
4:选一个 可编程的电源控制器
5:直接用ARM或者DSP或者FPGA加驱动器
并且我要的是控制芯片,不是这种内置FET的,能不能再帮我看看谢谢了
Hi
为什么不考虑用全桥移相来做?
用buck芯片2个并联来做,单个也1000w, 很有困难。
LTC3703+CSD19536+CSD19506(同步)+VER2923(电感);可以辅助ACS754LCB-050或者LT4356过流保护及浪涌抑制;负载复杂时还需要考虑远端补偿
不过对于2000W,一般用隔离拓扑,全桥或者推挽更好些
谢谢你的答复,很有用!另外我想问一下,你推荐的LM25116和LM5116的最大占空比是多少,我在Datasheet里面没有找到。
谢谢您的回复,我还想问一下,你说的第三种方法:外MOS加外驱动的:UCC27222预测栅驱动两路+控制器(UC3525/3842/3846等等)
怎么看这个控制器可以出180°相移的信号?并且UC3525占空比50%以下、UC3842是单输出好像都不行,怎么去找类似的芯片?谢谢~
D1+D2不能大于1?为什么?再说交错并联就是两个buck并联在一起,如果他们的占空比不一样还能并?
我们的这个交错并联在额定输出的时候两路的占空比都是0.81左右。
可能是你理解错我的问题了,我说的D1D2是两路buck各自的占空比,你说的D1D2是一路同步整流buck的占空比,是互补的。