用LM5015做一个15W左右的辅助电源,输入电压58VDC,驱动一个隔离变压器,和DEMO板画的很接近,连接电源后没有任何输出。
从内部框图来看,提供电源,并且把EN引脚电压配置到超过1.26V,是不是就应该在VCC端能测量到6.9V电压?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用LM5015做一个15W左右的辅助电源,输入电压58VDC,驱动一个隔离变压器,和DEMO板画的很接近,连接电源后没有任何输出。
从内部框图来看,提供电源,并且把EN引脚电压配置到超过1.26V,是不是就应该在VCC端能测量到6.9V电压?
临时从深圳买的LM5015芯片有问题,死活没动静。
从TI的申请的样片装上有基本输出,调试中。
感谢分享,建议以后从官方渠道获取芯片
wang wang hongxing 说:临时从深圳买的LM5015芯片有问题,死活没动静。
从TI的申请的样片装上有基本输出,调试中。