请问贵司是否有适合输入DC 10-30V输入,输出3.5V/35A的IC,我得联系方式是:qiufan689@163.com,手机:13925579586
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果是要求隔离,可以采用有源箝位芯片, UCC2897A, TI有提供一个18~60V转3.3V/25A的方案: www.ti.com.cn/.../pmp6753
这个芯片要求输入电压高出18V, 输出电流做到35A没有问题,可以在这个方案的基础上修改一下,效率很高的。国半的有源箝位芯片LM5025,输入电压要低一点,可以是13V, 也是可以选用的。
或者采用UCC28230, 做成全桥的架构:www.ti.com.cn/.../ucc28230evm 可修改相关参数。所以也可以选用UCC28950/3895等全桥芯片:www.ti.com.cn/.../pmp5410
DCDC的不隔离方案,建议使用LM25116, 最高耐压可到42V,Driver电流1.8A:www.ti.com.cn/.../lm25116 或者 www.ti.com.cn/.../lm5116
如果采用不隔离芯片,可以选用Ti的TPS40131, 可以参考EVM板设计:www.ti.com.cn/.../getliterature.tsp
这个设计是10.8~13.2V转1.5V/40A的设计,您可以修改参数以适合您的应用。