Other Parts Discussed in Thread: BQ24250, BQ24250EVM-150
采用bq24250作为锂电池充放电管理芯片,进行带负载实验时发现:
1)芯片空载时看,Vbat和Vsys工作正常,电压基本在4V左右;
2)芯片Vbat连接锂电池后,带负载,Vsys工作电压正常约3.8~4V;
3)芯片Vbat不外接锂电池时,Vsys只要带稍微重一些的负载,其电压就降低到约2.5V;
用ti官方提供的bq24250 demo板测试,有相同的现象。目前的设置是:
en1 = 0 , en2= 0, #ce = 0;个人参负载考了芯片手册,感觉设置应该是没问题的,因为单给电池充电,开发板的功耗约5V, 0.7A 。芯片不接锂电池,只接负载时,输入电压5V,电流是0.02~0.06A之间,输出电压为2.5V,有时更低,推断此时芯片基本没工作,开发板测试亦有相同现象。
从bq24250芯片手册上看,该芯片的Vsys可以支持高达4A的输出电流,因此Vsys外接几瓦特的负载,应该是能正常工作的,所以非常疑惑,在手册中也没找到相关的解释。困扰很久了,跟代理反馈了一下,代理也不清楚,麻烦相关人士能给解答一下,谢谢!