This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2678中的webench模拟 与提供的数据回答矛盾

关于图1: 其中我所标注的1,2,3,4 分别代表的什么参数,可以提供详细解释的链接吗? 关于图1中的3,4都是IC-die,他们后面数据的区别?

关于图1中3,4和图2中1,2 对比,说明在24V到5V发热比16V到5V多,这是一个通用原则吗?(当输出电压恒定,输出电流恒定,电源管理芯片的电压降越多,发热量越大??)这个链接(www.deyisupport.com/.../10909.aspx)的回答是否有误 谢谢 希望可以提供详细的解释说明 

附件.zip
  • 你的仿真是否是分别在Vin=24V或者Vin=16V两个情况下的仿真,请按照Vin=16V~24V这个条件下仿真,然后确认在最小输入电压和最大输入电压下的热仿真,看芯片温度差异。因为后者的仿真,在硬件使用上条件是一致的,而前者却有所差异。

    图一中的3/4都是IC-die,没有明确定义,但是从功耗看,3是总功耗下芯片die的温度,后者是就单一芯片而言下的温度。

  • 补充一下,1指的是散热的风量和方向;2指的是板边缘的温度(默认热绝缘)。

    3和4的两个IC-die与该型号定义的热模型有关,看过数据手册也许您能猜到其含义,这里不方便公开。