Other Parts Discussed in Thread: DCP020505
输入引脚接5V电压没有问题,但是得不到想要的3V电压,输入端使用的是2.2uf电容,输出用的是1uf电容,syn引脚上拉和悬空都试过,结果一样,都是空载时输出5.5,接负载(单片机最小系统)时4.3V,离需要的3.3还差好多
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
空载和轻载输出电压偏高是正常的,即便空载到达5.5V以上。
建议再这个隔离芯片后再增加一个LDO. (TI的类似的DCR01系列就是芯片内部集成LDO,但是最大输出功率只有1W,可能不满足您的需求,而DCR02系列没有5V输入的)