This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504给单节磷酸铁锂电池充电

Other Parts Discussed in Thread: BQ25504, BQ24650

准备采用BQ25504给单节磷酸铁锂电池充电,VBAT_OV=3.75V。如果光电池板的输入>3.75V时,我看的资料是升压充电器要关闭,这是意味着此时光电池板不能给磷酸铁锂电池充电了吗?此时磷酸铁锂电池电压可能要远< VBAT_OV=3.75V。望TI专家解答。

  • 1. 你的光电板会有这么高的电压吗?若是这么高的功率的光电板给单节磷酸铁锂电池充电,Bq24650可能更适合你!你的光电板的具体情况如何?产品设计要求如何?

    2.  超过了VBAT_OV电压点,Boost肯定是要停止工作的,但是这个VBAT_OV是指VBAT脚的电压,也就是你被充电的电池是否过压

  • 1、我的太阳能板光照足够时输出5V以上,阴天时降到1~2V,产品设计要求是尽量利用光电板能量。

    2、我现在的方案是检测太阳能板输出电压VS,如果VS>3.8V,则不使用BQ25504而是使用其他的芯片来给磷酸铁锂电池充电。

          如果VS<=3.8V,则使用BQ25504来给磷酸铁锂电池充电.采用继电器来切换。

         

                                       这个方案不知有无不妥之处