Other Parts Discussed in Thread: LM5119, TPS40170, LM5117, UCC28019
你好,还请帮忙推荐一款IC.
synchromous buck controller, 输入 0-60V, 输出24-54V, 200W. 自己用外置运放做CC,CV 控制。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
功率太大的话建议用LM5119做交错并联BUCK,可以去TI.COM搜索LM5119然后有Webench设计。
这个设计中, 60V转54V需要大duty和小minimum off time。这个方面最合适的是TPS40170, 这个芯片最大60V。
最大65V的方案是,LM5117和LM5119。它们的minimum off time更大一些,要求开关频率低一点。
这个设计建议开关频率低于300kHz
你好,非常感谢您的回复。
另外我还有个问题想请教下。
如下设计 90-305AC, 450V DC 输出的PFC,200W 方案,从效率上来看,是选用连续模式的IC, 比如UCC28019好呢,还是选用 准谐振的IC 比较好呢。
Thanks