This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DCDC效率与散热的深究

Other Parts Discussed in Thread: LM25085, TPS53513, TPS53318

本人现在正在做一款激光恒流源,DCDC部分要求输入12V,输出2.3V 5A给后续恒流源供电,输出电压2.3V的原因是恒流部分使用MOS管进行线性调整,电压太高MOS管功耗太大。

现在遇到的问题是,我用LM25085做DCDC转换,输出2.3V 5A的时候,开关管和续流二极管发热严重,要求是在环境温度30度的时候,不超过55度。

MOS管导通电压-1至-2.5V。导通电阻25毫欧, 续流二极管5A的时候VF=0.4。已近比较小了。麻烦各位帮忙分析一下

我现在有两个方案:1.使用同步整流。

                                     2。继续死磕。因为我觉得可能是我反馈做的有问题,用示波器看MOS开关信号,比较杂乱。