Other Parts Discussed in Thread: DCR010503, ISO15, ISO124, DCR010505
你好
我用UCC28910 输入市电,输出正负5V,如PMP9608参考设计,
再接DCR010503做转3.3V做隔离电源, 做了几组电路,发现部分几块电路输出电压有些异常现象,
送电一开始5V电压会先上升至3V多,过几秒才稳在5V, 将问题电路的DCR010503移开,
单独UCC28910电路加负载测试,电压正常稳压就没这种状况发生
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
DCR010503的负载时什么?
将没有问题的 DCR010503,更换到有问题的 DCR010503 板子上, 不良现象是否重现?
Hi,
谢谢各位的回答, 我认为是DCR010503的问题, 确实是只有其中几组板子有问题,
且跟换部分DCR010503有好转, 详细问题我也不清楚, 才会上来发问讨论是否为正常现象,
DCR010503的负载为ISO15做隔离测电源