Other Parts Discussed in Thread: LP5912, TPS7A49, TPS7A30
TI工程师们:
你好!帮忙推荐以下2个设计方案
1. 12V转-5V一个方案,要求输出电流可以很少不低于200mA就行,但输出纹波要求非常小,最好是低于0.5mV,功耗也希望尽可能地低;
2. 12V转5V的LDO设计方案,输出电流150mA左右就行,但考虑到有7V的压降,可能对IC的温升是有一个极大影响,也在思考如何处理这个问题。
以上,还请各位帮忙推荐,十分感激!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.