Other Parts Discussed in Thread: TPS54350, TPS54622, TPS54620
如果我用TPS54350的时候, 当输入电压为6V-12V, 输出为5V, 电流2A左右, 有没有问题呢? 输入最小为6V时, 输出5V, 是否压差太小了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应该是不行,输入6V时输出最大只能到4V左右。详见数据手册图48.
建议采用高效率的同步整流芯片,推荐TPS54622。这样无论是重载还是轻载都不会有Low Drop Out的问题。
你也可以在www.ti.com.cn/.../homepage.tsp 用Webench帮助选型和仿真。
多谢。 我也通过SwitcherPro软件确认了这个问题, 请教一下, TPS54622和TPS54620是什么区别?
Jinhong,
TPS54622和TPS54620的主要区别:TPS54622多了一个hiccup current limit的功能,并且有更低的参考电压。
两个芯片都是同步buck, 参数也比较接近,主要的差异在与参考电压,TPS54622是0.6V, TPS54620是0.8V, 另外就是OCP过电流保护的差异,TPS54622支持打嗝模式的电流保护,具体描述见两个芯片datasheet第十六/十七页Overcurrent Protection的描述。