Other Parts Discussed in Thread: TPS53319
TPS53319做3.3V10A输出没有问题,更换PCB布线输出载5A以后电压从3.3一直降到2.9V(10A的时候),且在新版本12V输入开机不能满载启动(旧版本可以)。新版本为两层板,旧版版本为4层板(中间两层为地线)。请问下这个问题除了该PCB板有没有什么好的建议(PCB的改版对那个地方的影响造成了该现象)?谢谢!~~





This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS53319
TPS53319做3.3V10A输出没有问题,更换PCB布线输出载5A以后电压从3.3一直降到2.9V(10A的时候),且在新版本12V输入开机不能满载启动(旧版本可以)。新版本为两层板,旧版版本为4层板(中间两层为地线)。请问下这个问题除了该PCB板有没有什么好的建议(PCB的改版对那个地方的影响造成了该现象)?谢谢!~~





你这个问题因为只是牵扯到PCB板改版,而原理本身没有什么变化所引起的,所以主要问题还是因为Layout的原因影响造成的!
具体Layout上你需要注意的是因为你改成了两层PCB,所以从电感L1和输出电容到负载的铜皮要加得足够宽,以10A为例,线宽要不小于12mm,同时输出电容的接地回到IC1 的 Pin23脚的铜皮也是同样的要求,要求宽,而且要尽可能的短,然后你VFB脚的反馈线采样点尽量靠近负载方向,因为你现在单层铜皮走线,10A的负载时在铜皮上的压降也不可小看,所以你看到10A输出时电压测到只有2.9V,很有可能就是被铜皮压降吃掉了,重点要关注这两点。
这么大功率做两层板挑战确实很大!另外GND脚接的散热铜皮也要尤为注意尽量做大面积,太热也影响IC的工作稳定性!
Hi
功率回路没有做好,比较两次的layout应该可以看到差异。