Other Parts Discussed in Thread: EMB1499Q
EM1401项目中在电源模块,每个电源设置独立的使能信号,请问这么做的意义在哪?我是否可用几个DCDC实现这几个电源呢?望回复。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通常来讲是为了整体功耗的控制,主动均衡模块在需要的时候进行启动,可以在不需要的时候把整个模块关闭,只保留AFE的监控功能等。你使用几个独立的DCDC电源也是可以的,只不过需要统筹考虑下板子的功耗而已。
这个当然是没有任何问题的,实际上目前很多客户量产的方案就是这样子的。
tang工你好,关于变压器选型问题,EM1401项目14串电池选的是750311492这个变压器,匝数比3.5:1,我们项目是12串的按照1499datasheet计算出匝数比为3:1,是否可以直接选用750311492这个变压器并通过调节其他参数实现目标输出呢?
Transformer Selection
The EMB1499Q is designed to work optimally with a transformer turns ratio of 3.5:1 when operating within a
stack of 14 cells. In order to maintain proper peak currents and voltage stresses on the drains of the power
MOSFETs, it is recommended that this relationship between turns ratio and number of cells be maintained. In
other words, follow the following equation when choosing a turns ratio for the transformer:
n = 0.25 x NumCells