This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650温度检测问题

Other Parts Discussed in Thread: BQ24650

请问BQ24650温度检测脚TS的VLTF、VLTFH、VHTF、VTCO的标准电压分别是多少?我们样机0℃时,当TS脚电压为2.436V时充电停止,升温VTS=2.399V时恢复充电。40℃时VTS=1.453V时充电停止,降温VTS=1.570V时充电恢复。这些数据符合要求吗?

看到计算工具里面设置的是1.49V~2.43V,1.453与1.49比较偏差较大。