我按照TPS54531数据手册设计的5V输出电路,稳定情况下12V输入,电压输出在5.14V,这个我觉得还是正常的。
现在的问题是,我在刚加电的瞬间,输出电压能够到6V多,这个问题应该怎么解决呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我按照TPS54531数据手册设计的5V输出电路,稳定情况下12V输入,电压输出在5.14V,这个我觉得还是正常的。
现在的问题是,我在刚加电的瞬间,输出电压能够到6V多,这个问题应该怎么解决呢?
Hi,
您指的是上电启动瞬间输出电压过冲会达到6V多,然后稳定在5.14V对吗?如果是这样的话可以通过两方面优化:
1. 增加软启动时间,即4脚电容增大
2. 改善环路,使系统响应变慢。即可以增大零点电容(补偿网络中和电阻串联的电容)
谢谢~
Regards,
Patrick