Other Parts Discussed in Thread: BQ24090
ISET连接的1K电阻,ISET2接地,按理应该按照ISET设定的电流充电,大概500ma,可是给1200mah的电池充电电流只有70ma左右。
还有CHG引脚接的LED亮是代表充电完成么?
英文能力有限,谢谢大家
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
忘说了,那个二极管和双向稳压二极管都没有焊接,没有短路。我这有三块实验板,都出现了这个问题,电阻我都测了,没问题。
CHG引脚我明白了,但是在接CHG引脚的LED灭的时候却还有70ma的电流充电,并且电流不稳,在这个状态下,测得输出电压4V。我测电流的方法是直接用万用表串联的。
我把ISET2接的10K电阻拆了,使ISET2悬空,再次充电,测得电流80ma,电流是个稳定值,接CHG的LED灯也亮了,正常充电。
但我想提高充电电流,这样充电太慢了。ISET接1K电阻,ISET2接地,按理应该充电的电流大概是500ma,但就是不能正常充电,接CHG的LED不亮,电流也才70ma,这样冲了一天,1200mah的电池才充到3.8V。
明天再去测试一下ISET2接高能不能解决问题吧。。。