Other Parts Discussed in Thread: BQ24070, LM26001
TI大神:
由于项目需求的需要,现在添加锂电池充电模块,供电电压在3到30V之间不停的变化,求大神推荐款合适的锂电池充电芯片,通过提供的供电电压,使用 充电芯片对锂电池进行充电,完成项目需求,谢谢大神的解答
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ24070可以。
你的输入电压范围太宽了,确定需要最低电压到3V吗?
如果必须的话,可以用LM26001做一个升降压线路到-5V输出,BQ24070的地接-5V输出,VIN接LM26001的地。线路类似以下的应用手册: