Other Parts Discussed in Thread: TPS54383
大家好,我最近使用TPS54383 24V输入12V和5V输出时,12V输出端(SW1)正常,5V输出端(SW2)波形异常,2路规格参数是一样的。原理图和波形见下:
SW2波形
理想的波形应该为这样。
我尝试着更改5V后端的滤波电容从100uF改为200uF以及更改采用电阻的走线,结果一样,谁请帮忙分析一下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.