Other Parts Discussed in Thread: TPS43000, TPS55340, TPS61087, LMR62014
我的系统采用3.7V锂电池供电,是一个手持便携设备,类似手机。但是有一部分电路是采用7.4V供电的(射频功放),因此我需要从3.7V升压到7.4V。7.4V那部分电路峰值电流不超过1.5A。
请推荐一款DC-DC芯片。要求:集成度高,输出噪声小。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
再您的应用中因为是采用电池供电,因为要考虑到电压电压下降,所以需要考虑到较低的输入电压情况下工作,而且输出电流需要达到1.5A的峰值,推荐TPS43000 .采用升压架构,外置MOS.
哦,不过这个个头好大。我们是便携产品,对体积还需要稍微考虑。我自己查了一下,TPS55340这个好像也能满足。。不知道你有什么建议?
TPS55340是可行,但是它的最低输入电压时2.9V, 设计方法可以参考datasheet: www.ti.com.cn/.../getliterature.tsp 之boost架构。
TPS43000,占用空间比较大,但是可以实现较低的输入电压。
如果考虑到空间使用,您是可以选择TPS55340的。
TPS61087能满足你的要求,1.2M开关频率可以使用小尺寸电感, 内部集成开关管且外围器件少。
谢谢楼上几位。电源方面我不太懂。我用Ti官网上提供的Excel表格来算了一下TPS55340的外围器件值,在附件中,可否帮我检查一下是否有问题。我电路的要求如下:
1,输入电压范围:3.5~4.2V
2,输出电压:7.4V
3,电路整体体积尽量小(电感我选择了2.2uH)
4,输出电压的纹波尽量小(输出电容我选了约100uF,是不是越大越好,我还可以选超级电容来滤波)
你好。TPS61087输出电流出1.3A会不会比较吃力?我看这个整体尺寸是比TPS55340小一些。
TPS61087输出电流达不到1.3A, 建议还是用TPS55340.
Johnsin你好
帮我看看我上面回复里的设计是否合理吧。谢谢。
对于上述的设计,因为您的频率设计得比较高1.2MHz, 所以计算所得电感比较小,可以选择2.2uH电感,但是这样会导致效率相对偏低.
输出电容并非越大越好,主要在于输出电容满足最小容值要求,同时满足ESR要求,datasheet参考设计采用3个47uF的电容并联就是为了得到较小的ESR, 以达到较小的输出纹波的目的。
谢谢Johnsin的回复
1,这个设计对效率不是很敏感(DCDC常态为关闭状态,需要用7.4V时才打开DCDC)。所以可以不考虑效率问题。我有关于电感选用的疑问:是不是我应该选用磁屏蔽的电感?
2,为了得到极其纯净的7.4V电压,电容加的很大不好吗?是不是有最大值的限定?我计划用超级电容来滤波,比如0.1F。同时会并联几个47uF的电容来满足ESR的要求。这样会有问题吗?
电感选用DC/DC转换的功率电感即可,只要注意饱和电流够就可以了。
输出电容够就好,并不是越大越好,要得到较为纯净的7.4V还可以再增加LC滤波。
推荐使用LMR62014
1,输入电压范围:2.7~14V, 最高输出电压:14V
2,芯片SOT23-5封装(<3*3mm2),方案体积小于15*15mm2.
3,开关频率1.6MHz,芯片内部补偿,内置MOS
4,开关电流最大达1.4A
客户的需求是输出的峰值电流在1.5A左右, LMR62014是开关峰值电流1.4A, 实际输出电流比较小,按照3.7V输入,7.4V输出,输出电流大约在400mA左右。