Other Parts Discussed in Thread: UCC2897A
各位老师好!最近用UCC2897A设计了一个有源钳位正激变换器,发现空载时候损耗非常大,而且大部分损耗来自变压器,但是满载效率还不错能达到92+,是什么原因呢,我设计的具体参数如下:
输入电压;36-72v 输出电压12V 输出电流10A 开关频率为300K 设置最大占空比Dmax=0.65 △B取0.4T 采用的磁芯规格是PQ2016,材质是PC40国产磁芯 AE=62 嵌位电容用的是0.47NF 250V
根据变压器公式Np=Vin min*Ton max /△B*AE=35*2.16/0.4*62=3T ,Ns取2T,辅助供电绕组Na=2T;绕线的电流密度大约为6A/mm2
做出样机测试发现空载损耗非常大,36V输入时,输入电流有0.15A,损耗达到5.4W,并且损耗绝大部分来自变压器,MOS管部分温度不高;带负载测试输入50V时候带载10A,测试效率能达到92+%;
以上参数是否合理呢?特别是△B取0.4T是否过大(有源嵌位正激变换器工作在1,3象限所以△B=2Bsat)? 是不是选择的磁芯质量不行或者磁芯选择过小,已经买了几个TDK的PC44磁芯来测试,样品还没有到?还是有其他原因呢,功率管驱动信号都不错;