大家好,在利用UCD9222+UCD7424做电压源的时候,发现电压输出很不稳定,为了防止将芯片烧坏,将输出电压设置为0.2V,这是发现输出电流变化非常大,参看下图,请问为什么电压变化不是那么明显的情况下,电流可以发生这么大的变化呢?我后面已经接了负载了是DSP,经测量发现电压供应端和地之间也就十几欧姆的电阻,请问这是为什么?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Guoping,
你可以观察电流采样的AD口,看这个信号是否稳定,这样可以验证电流采样电路是否有问题。
你好,专家LI,我的设计中采用UCD9244来控制两个UCD7242,期待四个RAIL都输出动态1V的电压,电流是10A,可是在Fusion Digital Power Designer软件里不知道怎么配置参数,我配置的输出上板卡后都是在0V左右波动,显示错误是电压过大,FLT错误等等,另外还有PMBUS的CNTRL引脚手册上说是拉高,可是参考设计上却是拉低的,不知道有啥影响,希望专家能给一份参考的UCD9244的配置文件,或者以我的参数帮忙配置一下,发给我,希望有人可以回复我,各种欢迎,不胜感谢~ 另外附上我自己配置的文件,专家帮忙看下问题在哪奥