This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40211-***

Other Parts Discussed in Thread: TPS40211

用TPS40211做了一款电源,输入12V-18V,输出为16V的DCDC电源,用于驱动LED,输出1.3A。

但是在测试时,发现输出一直不正常,具体表现如下:

1、空载输出,电压正常。

2、带载后,无输出电流。电子负载设置CV电压是多少V,显示输出端电压就是多少V,但是没有电流输出。

3、当设置输出电压为12V时,有输出电流0.3A;输出电压为11V时,输出电流为1.2A;输出电压为10V时,输出电流为变态的2.7A。

请问,这种情况该如何去排查及处理。感觉TPS40211这颗料,全被的控制集中在PIN5上,这一点真心难受,受影响因素太多了

附件文档是原理图及PCB板,使用软件AD13

double small-board.rar