Other Parts Discussed in Thread: UCC2897A, LM5020, LM5025
您好,麻烦请推荐一款DC/DC 隔离电源芯片。
输入:DC -38~-72V
输出:12V/5A
效率:85%min
工作温度:-40~70度
Surge: 6KV at CM
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好
那我输入是反着接给IC供电是吧?
UC2897A做的是有源钳位正激?
没事,你就按照正电压来设计就好了,输出反正跟输入没什么关系
对的,是正激电路。 反激的话可以看看LM5020
Hi
类似的设计案例: http://www.ti.com.cn/cn/lit/df/slur851/slur851.pdf