Other Parts Discussed in Thread: TPS54331, TPS54360, TPS54340, TPS54060
我想做一个应用是,输入24V,输出-12V,1A以下电流,请问TPS54331可以做嘛?有没有原理图参考,十分感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
降压芯片都可以做成负压输出的,但是按照24V转-12V,压差36V,故你需要选择36V以上的降压芯片,例如TPS54340, 或者TPS54360:
见设计文档:http://www.ti.com.cn/cn/lit/an/slva317b/slva317b.pdf
注意最大输出电流是要打折扣的。
Hi
TPS54360是TPS54060的3.5A输出版本,TPS54340是TPS54360 42V输入版本,都是差不多的。
你好,经过对比,还是TPS54331性价比高,你提到的耐压问题,我想能不能这样,方案改成正负5V输出。先用24V转成5V,再用5V转成-5V。。那么负压输出电路是和正压输出电路是一样嘛,或者有无原理图可以分享一下?我看TPS54331的手册没有提到负压输出电路,十分感谢。
Hi
TPS54331耐压只有28V, 肯定不行。
你需要的正负5V或者正负12V, 最大电流是多少?
HI
用TPS54360 这样的降压芯片加耦合电感,整体成本肯定要低一点,只是看能否找到符合条件,价格又比TPS54360便宜很多的芯片?
你好,正负12V方案成本太高,我想改成正负5V方案,所以我是想用一只 TPS54331(24V输入,5V输出(1A) ),然后再用另一只 TPS54331(5V输入,负5V输出(300MA) ),,这样可行吗?
你好,负压的生成电路以及元器件参数,跟正5V输出的一样嘛?