This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

QB25101

Other Parts Discussed in Thread: BQ25101, BQ25100

HI TI 专家您好,有关于BQ25101充电指示灯相关的问题

我参考如下的设计链接电源指示灯,灯的正极接Vin,负极接CHG,Vin为标准的USB充电器,但是现在发现接上充电器以后,LED灯常亮,当电池充满以后,充电指示灯不会灭,我量测CHG电压为,0-1.8V,请问这个是哪里有问题,

  • 1. 请确认是否用的是BQ25101, TI的BQ25100跟25101是P2P的,只有PG这个脚功能不同。如果拿错芯片了,可能会有这个现象。

    2. 如果芯片没错,是否是因为电池实际还未充满:尽管电压已经到位,但只是CV模式,电池充电还没结束。

  • zhengxing,非常感谢您的回复

    1. 请确认是否用的是BQ25101, TI的BQ25100跟25101是P2P的,只有PG这个脚功能不同。如果拿错芯片了,可能会有这个现象。

    -->这个料号为BQ25101HYFPR,这个也是供应商提供给我们的,而且我们一次也买了一盘2000pcs,这个有什么办法我可以辨别吗?

    2. 如果芯片没错,是否是因为电池实际还未充满:尽管电压已经到位,但只是CV模式,电池充电还没结束。

    -->这个我充了大概有12个小时,充电电路为150mA,电池容量为300mAH,而且目前我测试10个,CHG的最大电压都是为1.8V,如果是正常情况下,BQ25101电池充满以后CHG得电压为多少V,

    期待您的回复~

  • 1.是否发错货,得找供应商确认。另外,可以TI官网申请一些BQ25101的样品,试下。

    2. 是否是TI的EVM上测的?PG信号是否连接到其他电路,如果有,去掉其他电路看看。