5.5V时PTH12040输出的最大电流能到多少,如果用2个这样的模块并起来用的话,最大是不是可以达到90~100A?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
5.5V时PTH12040输出的最大电流能到多少,如果用2个这样的模块并起来用的话,最大是不是可以达到90~100A?
5.5时PTH12040输出电流可以达到50A, 但是如果您的应用需要两个模块并联,需要用到均流,是可以达到90~100A。如果不用均流,容易出现其中一路电流过大超过(50A), 而另一路电流过小。
PTH12040W的最大输出电流与环境温度有关,不是所有情况下都是50A。详见数据手册图3。
另外PTH12040W本身已经采用三相结构,但是数据手册中并未提及可以多模块并联,因此可能会出现Johnsin提到的问题。
确实要关注温度问题, 所以要50A输出是可以的,但是要注意一些条件如环境温度,功耗,风速等等。