刚买的EV2300和bq3060-evm,接上两节磷酸铁锂电池测试,在PACK+和PACK-之间电压为0,在bq3060EVSW软件中没办法改写DataFlash,要怎样才能改写DataFlash?谢谢了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Bin,
请短接 cell 2,3,4 的连接头,配置为两串需要将高串短接!因为 3060 的默认配置不是 2 串,所以现在是处于欠压状态, 放电 MOS 关闭,测试 P+,P- 电压为零正常。
因为 BQ3060 默认的 flash update ok voltage =7.5V .两串磷酸铁锂电芯的电压应该在 7.5V 以下,所以无法更改 dataflash. 可以先用稳压电压模拟电池把电压拉上来,更改 GG 文档,将 flash update ok voltage 调低后再上两串铁锂电池调试。