Other Parts Discussed in Thread: BQ24113, BQ24103
需要充电电压7.2V,标准充电电流140mA,最大充电电流1A的1400mAh的锂电池充电选型,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
James,
从你的参数看,应该是两个锂电池,标称电压为3.6*2=7.2V,但电池在充满电的情况下可能会达到4.2*2=8.4V,如果选用开关型的充电芯片,可以参考BQ24103,或BQ24113.