下面在附件是SN6501-5EVM评估板。变压器的具体参数能否提供,方便订购,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
该变压器页面:www.coilcraft.com/da2303.cfm
也可以联系Coilcraft索取详细参数
关于SN6501变压器选型可以参考datasheet: www.ti.com.cn/.../getliterature.tsp datasheet第十四页:TRANSORMER SELECTION :采用的是伏秒法选择变压器。
SN6501采用的是3~5.5V供电建议采用5V,输出可以达到1W以上), 此时伏秒值为9.1V*uS,选择9.1V*uS以上的变压器即可。
关于匝数,参考datasheet第十五页的方案:
VS-min = VF-max + VDO-max + VO-max = Vout
VP-min = VIN-min - RDS-max x IDmax = Vin
最小匝比Nmin= 1.031*Vout/Vin