This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

设计一个工业上使用的电源,哪种合适?

Other Parts Discussed in Thread: TIDA-00118

我的设计要求是这样的:PLC监控线路是否工作正常。采用空心型电流传感器采集信号(在传感器两端并联一个电阻),信号幅度从20mV到500mV(根据采集的电流大小不同)。

这样电压信号思路是这样的,首先采用INA128和OPA188(从TI网站上找的参考设计),放大5倍;然后在通过由OPA2180组成的二阶低通滤波器,然后再经过OPA180组成的放大倍数可调的放大电路;输出信号在+/-4V左右,再通过LM211迟滞比较电路,出现0-12V的脉冲波形,最后经数字光耦TLP521输出0-24V脉冲波给PLC,PLC通过检测有无脉冲波叛变线路是否正常工作。

这里面要设计一个工业使用的电源,输入电源是开关电源提供的+/-24V。电路中有精密仪放芯片,所以要用+/-5v电源,其他运放芯片想用+/-12V电源,这样就不会干扰到仪放的使用。我也看到你们参考设计了,不过好多,哪个适合?我主要是滤除各种频率干扰。开关电源的话里面会有高频干扰,用LDO的好点,也要用ISO电源隔离吗?本来想用78,89系列的,先降到12V,再降到5V,但太热,长时间工作怕出问题。请求帮助!

Doc1.docx