This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27200中LMD更新的值是根据什么判定的

Other Parts Discussed in Thread: BQ27200

bq27200中LMD更新的值是根据什么判定的

  • 简单的说是,完整的电池满充到放空过程中的库伦量。

    具体参考 http://www.ti.com/lit/ds/symlink/bq27200.pdf page 10

  • 你好,文档我都看了,但是有些不是很确定,因为在实际测量过程中有些不太一样;请问,芯片默认的LMD值为2d,也就是说电池电量为2000多毫安时,默认的EDV1=3250mV,我用12000毫安时的电池充满放电时VDQ=1,NAC=LMD,当NAC=LMD/16时,NAC的值不再减小,但在Vbat没有达到EDV1的值的时候VDQ就清零了,这种现象对吗?

  • 你好,文档我看过了,按照里面的说法,当我把电池充满后FLAGS寄存器中的IMIN位会清零这属于正常的,此时我放电FLAGS寄存器的值为0X14应该也没有问题;

    我设置的EDV1的值为3400mV(按照eeprom更改方式在PGM管脚21V电平),放电时lmd的值为0x2d00默认的,当NAC将到LMD/16时会维持好长时间不变,正常情况是电池电压降到EDV1的值时会完成电量学习,然后flags会成0;但是总是到3.6V左右时FLAGS的VDQ位清零,并且没有出现不良放电情况,此时CYCL值为7,我电池容量大概为12Ah,我测试的几台设备中有能正常完成的,不正常的原因有哪些呢